你好:
CC2591有三个脚与CC2530连接,如果硬件管脚连接的是其他的管脚则需要在协议栈上修改。值得注意的是PA_EN与EN只能连接在P1_0到P1_5,这是由CC2530决定的。HGM可以任意定义。
上面红色字体是说,PA_EN与EN只能连接在P1_0到P1_5 是只能这样配置么
我的PA_EN,EN,HGM分别接cc2530的P0_0, P0_1, P0_2这三个引脚.理由是什么呢? 电路图如下
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
不可以的。建议参考文档 http://www.ti.com/lit/an/swra290/swra290.pdf
1) P0_7 can be moved to any GPIO pin, and the macros below HAL_PA_LNA_RX_LGM() and
HAL_PA_LNA_RX_HGM() must be modified accordingly.
2) P1_1 and P1_4 are a subset of GPIO pins (only P1.0-P1.5) that can be configured to
support special RF observation output control signals.