Other Parts Discussed in Thread: CC2590
在PA 模式下, HGM_EN 为什么初始化为三态呢》?
#elif defined (HAL_BOARD_CC2530EB_REV13) || defined (HAL_PA_LNA) || \
defined (HAL_PA_LNA_CC2590)
#define HAL_BOARD_INIT() \
{ \
uint16 i; \
\
SLEEPCMD &= ~OSC_PD; /* turn on 16MHz RC and 32MHz XOSC */ \
while (!(SLEEPSTA & XOSC_STB)); /* wait for 32MHz XOSC stable */ \
asm("NOP"); /* chip bug workaround */ \
for (i=0; i<504; i++) asm("NOP"); /* Require 63us delay for all revs */ \
CLKCONCMD = (CLKCONCMD_32MHZ | OSC_32KHZ); /* Select 32MHz XOSC and the source for 32K clock */ \
while (CLKCONSTA != (CLKCONCMD_32MHZ | OSC_32KHZ)); /* Wait for the change to be effective */ \
SLEEPCMD |= OSC_PD; /* turn off 16MHz RC */ \
\
/* Turn on cache prefetch mode */ \
PREFETCH_ENABLE(); \
/* LED_1 P10 EZMODE STATE LED_2 P12 NETWORKSTATE */ \
LED1_DDR |= (LED1_BV | LED2_BV ); \
\
/* Set PA/LNA HGM control P0_7 */ \
P0DIR |= BV(7); \
\
/* configure tristates */ \
P0INP |= PUSH2_BV; \
\
/* setup RF frontend if necessary */ \
HAL_BOARD_RF_FRONTEND_SETUP(); \
}