This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
下载Z-Stack 3.0.2后,打开目录下的D:\Texas Instruments\Z-Stack 3.0.2\Projects\zstack\ZNP\CC253x 的znp.eww后,修改linker ---option----output, 可编译生成hex文件,烧录后,上电程序可以运行(加了一个LED灯和串口),但是通过空中抓包工具Ubiqua, 发现这个ZNP没有创建网络,不知为何?
以前用的ZHA1.2.2a是没问题的。
查看程序发现zigbee3.0的void ZDApp_Init( uint8 task_id )函数中无 ZDOInitDevice( );
知道zigbee3.0新增了BDB,但是这个ZNP怎么不能创建zigbee网络,需要怎样让它作为一个协调器建立一个zigbee网络。
希望得到TI大神解答,谢谢!
您好,
zigbee3.0使用的Base Device Behavior(BDB)来进行网络的初始化和设备的配置。
ZDOInitDevice( );被更为bdb_StartCommissioning
您好,谢谢回复!在Z-Stack API.pdf的3.4.1没有看到关于这方面的说明。这个3.0的ZNP默认不是协调器吗?默认不会建立网络吗?企业微信截图_17020061089135.zip
您好,我在初始化最后直接增加了:
bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_FORMATION | BDB_COMMISSIONING_MODE_FINDING_BINDING|BDB_COMMISSIONING_MODE_NWK_STEERING);
2,把znp.cfg 文件修改为:
/* Generic All-in-One Settings */
//-DZSTACK_DEVICE_BUILD="(DEVICE_BUILD_COORDINATOR | DEVICE_BUILD_ROUTER | DEVICE_BUILD_ENDDEVICE)"
-DZSTACK_DEVICE_BUILD="(DEVICE_BUILD_COORDINATOR )"
ZNP还是不能建立网络,要如何解决?谢谢
3,不知道是否还要把f8wCoord.cfg文件add 到tools中,也测试了,加入后,也没用。
/*
* f8wCoord.cfg
*
* Compiler command-line options used to define a TI Z-Stack
* Coordinator device. To move an option from here to the project
* file, comment out or delete the option from this file and
* enter it into the "Define Symbols" box under the Preprocessor
* tab of the C/C++ Compiler Project Options. New user defined
* options may be added to this file, as necessary.
*
*/
/* Common To All Applications */
-DCPU32MHZ // CC2530s Run at 32MHz
-DROOT=__near_func // MAC/ZMAC code in NEAR
/* MAC Settings */
-DMAC_CFG_APP_PENDING_QUEUE=TRUE
-DMAC_CFG_TX_DATA_MAX=5
-DMAC_CFG_TX_MAX=8
-DMAC_CFG_RX_MAX=5
/* Coordinator Settings */
-DZDO_COORDINATOR // Coordinator Functions
-DRTR_NWK // Router Functions
4,怎么能让这个ZNP以协调器跑起来,谢谢!
bdb_StartCommissioning(BDB_COMMISSIONING_MODE_NWK_FORMATION | BDB_COMMISSIONING_MODE_FINDING_BINDING|BDB_COMMISSIONING_MODE_NWK_STEERING); 是被放在函数void znpInit(uint8 taskId)最后。
现在有一种可能性,是CC2530的设备被错误地设置为路由器或者是终端设备而不是协调器
BDB_COMMISSIONING_MODE_NWK_STEERING)
这一项使得设备将本机和其他具有相同PAN ID的设备连接到网络,而不是会创建新的网络
编译后的文件的程序是在跑的,LED可亮,串口也可收发数据
所以会出现以下情况
ZNP原本的用途就是要透過外部CPU/MCU利用ZNP/MT command创建zigbee网络,需要让CC2530直接作为一个协调器建立一个zigbee网络的話,建議直接使用samplelight例程