This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

zigbee 怎么通过mac地址获得网络中节点的短地址



各位大神:

            新年好,请问zigbee 怎么通过mac地址获得网络中挂在路由下的节点的短地址,APSME_LookupNwkAddr得到短地址时,只能查找协调器儿子节点,对孙子节点不可访问,

afStatus_t ZDP_NwkAddrReq( byte *IEEEAddress, byte ReqType,

                           byte StartIndex, byte SecurityEnable )

根据已知网络地址查询远程设备物理地址,作为一个广播信息发送给网络中的所有设备:这个函数也是知道IEEE地址,对短地址进行寻找,这个不存在上面所说的限制,但是这个短地址放在那里呢,我怎么获得这个短地址呢?