RT:我在使用TIMAC1.5.1中,想通过DMA的方式进行串口的数据收发,我做了如下操作:
在工程文件option——>c/c++ Compiler——>Preprocessor我将HAL_DMA=TRUE,xPOWER_SAVING;
但无法使用HalUARTWriter(),期待回复~~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
RT:我在使用TIMAC1.5.1中,想通过DMA的方式进行串口的数据收发,我做了如下操作:
在工程文件option——>c/c++ Compiler——>Preprocessor我将HAL_DMA=TRUE,xPOWER_SAVING;
但无法使用HalUARTWriter(),期待回复~~
1、首先如上面说的,修改工程option里面的宏;
2、我修改的配置文件内容如下:
#if HAL_UART // Always prefer to use DMA over ISR. #if HAL_DMA #ifndef HAL_UART_DMA #if (defined ZAPP_P1) || (defined ZTOOL_P1) #define HAL_UART_DMA 1 #elif (defined ZAPP_P2) || (defined ZTOOL_P2) #define HAL_UART_DMA 2 #else #define HAL_UART_DMA 1 #endif #endif #define HAL_UART_ISR 0 #else #ifndef HAL_UART_ISR #if (defined ZAPP_P1) || (defined ZTOOL_P1) #define HAL_UART_ISR 1 #elif (defined ZAPP_P2) || (defined ZTOOL_P2) #define HAL_UART_ISR 2 #else #define HAL_UART_ISR 1 #endif #endif #define HAL_UART_DMA 0 #endif
PS:因为先前程序有被我改过很多,不知道有没有影响,如果大家遇到这个问题,可以PM我,一起讨论 .