Other Parts Discussed in Thread: CC2530, Z-STACK, CC2538
我想请教一下,zigbee组网最多能支持多少个节点,我用的是CC2530,使用的协议是2007zigbee pro,目前安装了300多个节点,发现有些节点不能进入网络,在实验室使用108个节点,都可以进入网络。zigbee组网理论上可以支持很多节点,实际应用最多能支持多少,怎样修改协议可以增加组网节点数量?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
关于zigbee大规模组网,TI有一份专门的文档 http://www.ti.com/lit/an/swra427c/swra427c.pdf。您可以参考其中的相关设置。
谢谢你的回复,该文档对我们有很大帮助,该文档推荐在组建大规模网络时使用Many-to-One Routing Protocol协议,该协议在the Z-Stack Developer's Guide文档中有介绍,我没有找到这个文档,请问在哪下载这个文档呀,谢谢
在协议栈的安装文件夹内 C:\Texas Instruments\ZStack-CC2530-2.5.1a\Documents
同问下,300个节点是否是双向通信还是单向,另外网络配置了多少路由器,请教下,谢谢!
上诉文档中提到的方案【400nodes】用的是many to one,具体请参考文档
针对AN123 – Breaking the 400-Node ZigBee® Network Barrier With TI’s ZigBee SoC and Z-Stack™ Software这篇文章,有几个问题需要帮忙确认一下:
Victor Jiang 说:针对AN123 – Breaking the 400-Node ZigBee® Network Barrier With TI’s ZigBee SoC and Z-Stack™ Software这篇文章,有几个问题需要帮忙确认一下:
- 在这个400节点的网络中协调器用的是CC2530吗,具体型号是 哪个?
是CC2538- 400节点网络中有多少数量是路由(router)节点,多少数量是终端节点(end device)?全是路由
- 文档中Table 3. Per Hop Latency Statistics of the Test Network第二跳和第三跳设备数量176、175都是路由(router)节点吗?如果不是,每跳有多少终端节点?是的
- 我们准备用CC2530F256RHAR搭建一个协调器(coordinator)+250个路由节点(router)进行双向稳定通信(协调器间隔1秒查询全部节点并上报一次到协调器)是否可行?我们实际在一个200平方的房间内搭建一个协调器(coordinator)+250个路由节点(router)的网络时,用many to one组网时节点无法全部上报,会随机遗漏几个节点,产生这种情况可能的原因是什么?
比较困难,原因在于CC2530因为RAM限制,没办法保存到所有节点的路径,这也意味着在跟大部分设备通信的时候,都要通过路由请求来找路径,这个过程也是有一定的时间消耗的。
AN123里所用到的例程只是说明如何调整参数获得高达400的网络节点配置,实现功能也很简单,节点加入网络之后,协调器发送一个广播消息,节点按照配置的间隔传输数据包。这部分在文档的section3有解释