This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530 UART串口问题

        从datasheet上了解到,通过设置PERCFG可将UART0和UART1同时分配到P0端口,且禁用UART流控,从IO映射表看,此时UART0的RX,TX 使用P0_2,P0_3,此时UART1的RX,TX 使用P0_5,P0_4。

        问题来了,当设置P2DIR.PRIP0为00,即UART0优先时,在UART1串口上通过DMA方式发送数据,却发现无法发送;而当设置P2DIR.PRIP0为01,即UART1优先时,在UART0串口上通过DMA方式发送数据,也同样无法发送。想请教一下这是为什么?