This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530F128 芯片运行ZLL问题

Other Parts Discussed in Thread: Z-STACK

Z-Stack Lighting 1.0.2 + IAR 8051 9.10编译ZLLRC -EndDevice工程, 在芯片选择CC2530F256可以通过, 但选择CC2530F128就会出现如下错误

Error[e16]: Segment ZIGNV_ADDRESS_SPACE (size: 0x3000 align: 0) is too long for segment definition. At least 0x3000 more bytes needed. The problem occurred while processing the segment placement  
command "-Z(CODE)ZIGNV_ADDRESS_SPACE=_ZIGNV_ADDRESS_SPACE_START-_ZIGNV_ADDRESS_SPACE_END", where at the moment of placement the available memory ranges were "-none-"
   Reserved ranges relevant to this placement:
   CODE:3b4fb-3f93a     BANKED_CODE
   BIT:0-7              BREG
   BIT:80-87            SFR_AN
   BIT:90-97            SFR_AN
   BIT:a0-af            SFR_AN
   BIT:b8-c7            SFR_AN 

请教TI的工作人员,需要怎么样修改才能用CC2530F128这个芯片?