This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
查看api说明,有NLME_RouteDiscoveryRequest和NLME_NwkDiscReq2这两个函数尝试过实现标题的功能,在终端节点入网后去调用这些函数获取信息,跟踪调试结果只能获取到一个路由信息,除非周围还有其他panid网络的路由,而终端节点是0xFFFF的设置,那么就可以扫描到两个路由信息,仅此而已。
这个是哪里使用不档导致的?如何显示如上一个功能还请大牛们出出主意帮帮忙。现在我是使用路由节点1跳广播来路由设备上实现如上功能,终端节点还没能实现。
还有就是如何让已经入网的终端节点重新入网,选择新的父节点?使用NLME_ReJoinRequest并没有回调到ZDO_JoinConfirmCB里,好似没触发。
那就不要用NLME_RouteDiscoveryRequest了,直接用Scan就可以了。用NLME_DISC_SCAN
参考下面函数
/*********************************************************************
* @fn ZDO_ProcessMgmtNwkDiscReq
*
* @brief This function handles parsing the incoming Management
* Network Discover request and starts the request.
*
* @param inMsg - incoming message (request)
*
* @return none
*/
void ZDO_ProcessMgmtNwkDiscReq( zdoIncomingMsg_t *inMsg )
{
NLME_ScanFields_t scan;
uint8 index;
uint8 *msg;
msg = inMsg->asdu;
scan.channels = osal_build_uint32( msg, 4 );
msg += 4;
scan.duration = *msg++;
index = *msg;
scan.scanType = ZMAC_ACTIVE_SCAN;
scan.scanApp = NLME_DISC_SCAN;
// Save off the information to be used for the response
zdappMgmtNwkDiscReqInProgress = true;
zdappMgmtNwkDiscRspAddr.addrMode = Addr16Bit;
zdappMgmtNwkDiscRspAddr.addr.shortAddr = inMsg->srcAddr.addr.shortAddr;
zdappMgmtNwkDiscStartIndex = index;
zdappMgmtNwkDiscRspTransSeq = inMsg->TransSeq;
if ( NLME_NwkDiscReq2( &scan ) != ZSuccess )
{
NLME_NwkDiscTerm();
// zdappMgmtNwkDiscReqInProgress will be reset in the confirm callback
}
}
在完成Scan以后,会调用ZDO_FinishProcessingMgmtNwkDiscReq();函数,就可以把周围网络信息拿到了
@大神VV,可否直接调用ZDO_ProcessMgmtNwkDiscReq来获取数据呢?inMsg这个对象里的数据参数分别代表什么,如何造一个这样的参数来完成这次任务?
现在想先调试看看获取到啥,但是参数不知道如何造,卡住了。
另外,这个函数在API文档里没找说明,还真隐晦。
还烦大神打解下。谢谢
我设置了一个定时任务,直接如下代码调用函数
zdoIncomingMsg_t inMsg;
inMsg.srcAddr.addrMode = Addr16Bit;
inMsg.srcAddr.addr.shortAddr = 0xFFFF;
inMsg.wasBroadcast = TRUE;
inMsg.clusterID = 1;
inMsg.SecurityUse = 0;
inMsg.asduLen = 1;
uint8 asdu = 0xFF;
inMsg.asdu = &asdu;
inMsg.TransSeq = 0xFF;
inMsg.macDestAddr = 0;
ZDO_ProcessMgmtNwkDiscReq(&inMsg);
函数是进去了,可是没能在ZDO_FinishProcessingMgmtNwkDiscReq发现被调用到。是调用ZDO_ProcessMgmtNwkDiscReq的参数不对导致的还是其他什么原因?麻烦请VV大神解答下。谢谢
Hi VV:
手头上的一个项目需要解决的问题是:一个手持节点,可扫描当前区域内所有信道上的网络和网络ID号。
碰到几个问题,烦请大神指点一二。
1.在Scan后,调用ZDO_NetworkDiscoveryConfirmCB()函数返回networkDesc_t.寻遍整个工程都没有发现此函数在何处被显性调用的。难道此函数调用过程的源码未公开?
2.针对于函数NLME_NwkDiscReq2,技术文档上说:This function requests the network layer to discover neighboring routers. Use this function to perform a network scan but you are NOT expecting to join. The scan confirm (results) will be returned in ZDO_NetworkDiscoveryConfirmCB() callback. After the callback (results), call NLME_NwkDiscTerm() to clean up this action.
在进入ZDO_NetworkDiscoveryConfirmCB()函数立即调用ZDO_FinishProcessingMgmtNwkDiscReq()在对网络列表进行相应处理后终于调用了 NLME_NwkDiscTerm()函数,"clean up this action"。
我的问题是在NLME_NwkDiscTerm函数执
行后,ZDO_NetworkDiscoveryConfirmCB()函数后部分的代码还可以实现吗?如:ZDApp_SendMsg( ZDAppTaskID, ZDO_NWK_DISC_CNF, sizeof(ZDO_NetworkDiscoveryCfm_t), (uint8 *)&msg );也就是技术文献上说的call NLME_NwkDiscTerm() to clean up this action(req),清除了哪些呢?
3.寻遍整个工程都没有发现ZDApp_NwkDescListProcessing()函数的申明和实现。
Z-Stack版本:Z-Stacka-CC2530-2.3.1-1.4.0