Other Parts Discussed in Thread: CC2530, Z-STACK, CC2530EM
| 大家好,我想知道CC2530装入ZStack协议栈之后,CODE空间还剩多大,还可以存一个最大多少长度的数组,大概 |
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Memory sizes are shown below for the 3 ZigBee device types, with/without
ZigBee-PRO, with/without Security, and compiled to run on the SmartRF05EB
board with CC2530EM module. See the Z-Stack User's Guide for more details.
Coordinator Router EndDevice
PRO SECURE Flash/RAM Flash/RAM Flash/RAM
=== ====== ======== ======== ========
On On 158.4K/6.7K 158.2K/6.7K 128.2K/5.3K
On Off 149.2K/6.7K 148.0K/6.7K 120.1K/5.2K
Off On 147.1K/6.6K 146.9K/6.6K 121.9K/5.2K
Off Off 137.8K/6.6K 136.6K/6.6K 113.8K/5.2K