This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ZSTACK 2.5.1a 协调器无法发送无钱数据

经过几天的查找,终于出找到了错误。

协调器在使用AF_DataRequest 函数发送数据时,返回值为0x10。对应状态如下


#define afStatus_SUCCESS                            ZSuccess /* 0x00 */
#define afStatus_FAILED                                  ZFailure /* 0x01 */
#define afStatus_INVALID_PARAMETER     ZInvalidParameter /* 0x02 */
#define afStatus_MEM_FAIL                            ZMemError /* 0x10 */
#define afStatus_NO_ROUTE                         ZNwkNoRoute /* 0xCD */

请问TI 的前辈门如何解决这问题。

  • 您调用AF_DataRequest的频率是多少?如果调用频繁的话,确实会出现这种问题

  • 是这样的。协调器下有四个终端,每个终端以每6秒向协调器发一次数据,数据长度为5个字节。协调器在收到终端发来的数据后,会回5个字节。这样的算频率过快吗?

    产生这个问题,是在发送时,申请内存失败导致的吗?申请的是堆栈的3K内存吗?

    ****************************************
    * *
    * END OF CROSS REFERENCE *
    * *
    ****************************************

    162 963                       bytes of CODE memory
    32                                 bytes of DATA memory (+ 72 absolute )
    7 513                           bytes of XDATA memory
    192                              bytes of IDATA memory
    8                                   bits of BIT memory
    1 038                           bytes of CONST memory

  • 你程序里面是不是有动态申请内存,然后没有释放的,导致内存泄露的,你可以检查下。

    这个问题,是一开始会出现,还是运行一段时间以后才出现的?