Other Parts Discussed in Thread: CC2591
ZStack-CC2530-2.5.1a是我用的协议栈,我要用PA的功能
我做了如下修改:
1,修改hal_boar_cfg.h文件
把 #define xHAL_PA_LNA 修改成 #define HAL_PA_LNA
2.修改mac_radio_defs.c
#if defined HAL_PA_LNA || defined MAC_RUNTIME_CC2591
const uint8 CODE macRadioDefsTxPwrCC2591[] =
{
// 20, /* tramsmit power level of the first entry */这是协议栈默认的
1, /* tramsmit power level of the first entry *///这个是我修改的
(uint8)(int8)10, /* transmit power level of the last entry */
/* 20 dBm */ 0xF5, /* characterized as 20 dBm in datasheet *///我另外添加了一行
/* 20 dBm */ 0xE5, /* characterized as 20 dBm in datasheet */
/* 19 dBm */ 0xD5, /* characterized as 19 dBm in datasheet */
/* 18 dBm */ 0xC5, /* characterized as 18 dBm in datasheet */
/* 17 dBm */ 0xB5, /* characterized as 17 dBm in datasheet */
/* 16 dBm */ 0xA5, /* characterized as 16 dBm in datasheet */
/* 15 dBm */ 0xA5,
/* 14 dBm */ 0x95, /* characterized as 14.5 dBm in datasheet */
/* 13 dBm */ 0x85, /* characterized as 13 dBm in datasheet */
/* 12 dBm */ 0x85,
/* 11 dBm */ 0x75, /* characterized as 11.5 dBm in datasheet */
/* 10 dBm */ 0x65 /* characterized as 10 dBm in datasheet */
};
#endif
以下是PA功能开启
/* P1_1 -> PAEN */
RFC_OBS_CTRL0 = RFC_OBS_CTRL_PA_PD_INV;
OBSSEL1 = OBSSEL_OBS_CTRL0;
/* P1_2 -> EN (LNA control) *//
RFC_OBS_CTRL1 = RFC_OBS_CTRL_LNAMIX_PD_INV;
OBSSEL2 = OBSSEL_OBS_CTRL1;
----------------------------------------------------------------------------------------------------------------------------------------------------------
以上是我修改的协议 针对PA功能的,请问,还需要修改哪里吗?