Other Parts Discussed in Thread: CC2530
Hi
目前我想用CC2530 产生红外调制信号,我已经用timer3产生了38k的载波,但是我在用timer1产生调制信号的时候,没有成功。
我知道只用T1CC0产生周期,T1CC1产生占空比,为了改变调制宽度,没有T1CC1的compare up的ISR中通过CPU的方式更新T1CC1和T1CC0
当最后一次数据更新到timer1的寄存器后,在ISR中关闭timer1(T1CTL =0;),然而这一切并没有按照我所预想的执行。
我的代码如下,IR_data 是我的调制测试数据,麻烦帮我看看是哪里出了问题?
unsigned short IR_data[4]={0x0200,0x0100,0x0050,0x0500};
void main(void)
{
CLKCONCMD &= ~0x40; //设置系统时钟源为32MHZ晶振
while(CLKCONSTA & 0x40); //等待晶振稳定为32M
CLKCONCMD &= ~0x07; //设置系统主时钟频率为32MHZ
CLKCONCMD &= ~0x20; //时钟速度32 MHz 定时器标记输出设置[5:3]8MHz
CLKCONCMD |= 0x10; //时钟速度32 MHz 定时器标记输出设置[5:3]8MHz
CLKCONCMD &= ~0x08; //时钟速度32 MHz 定时器标记输出设置[5:3]8MHz
while(1)
{
if(P0_1 == 1)
{
MyDelay(100);
if(P0_1 == 0)
{
PERCFG |= 0x40;
P2SEL &= ~0x10;
P2DIR |= 0x80;
IR_data_index = 0;
time_tmp1=IR_data[IR_data_index++];
time_tmp2=IR_data[IR_data_index++];
T1CC1H = time_tmp1/256;
T1CC1L = time_tmp1%256;
T1CC0H = (time_tmp1+time_tmp2)/256;
T1CC0L = (time_tmp1+time_tmp2)%256;
T1CTL = 0x02; //module mode
T1CCTL1 = 0x1c; //set on compare , reset on 0,compare mode
T1CCTL1 |= 0x40; // 模式选择 通道1比较模式 使能timer1通道1的中断
T1IE = 1; //使能timer1的中断
EA =1; //使能总中断
}
}
}
}
#pragma vector=T1_VECTOR
__interrupt void T1_IRQ(void)
{
unsigned short time_tmp1 = 0;
unsigned short time_tmp2 = 0;
if(T1STAT | 0x02)
{
if(IR_data_index <4)
{
time_tmp1=IR_data[IR_data_index++];
time_tmp2=IR_data[IR_data_index++];
T1CC1H = time_tmp1/256;
T1CC1L = time_tmp1%256;
T1CC0H = (time_tmp1+time_tmp2)/256;
T1CC0L = (time_tmp1+time_tmp2)%256;
}
else
{
T1CTL =0;// stop timer
T1IE = 0;
EA =0;
}
}
if(T1STAT | 0x20)
{
}
}