This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

打开CC2591后两个节点不能通讯

Other Parts Discussed in Thread: CC2591, CC2530, Z-STACK

CC2591应该怎样配置才能接收到数据,我现在只要一打开CC2591,两个模块就不能通讯了,代码是参考basicRF改写的

  • 1)两块模块是不是放的很近,磁场饱和,详见datasheet

    2)测试下CC2591打开和关闭时模块的电流变化,看CC2591有没有工作;

    3)如果怀疑软件问题,建议可以试用2个仿真器试用smartRF studio配置发送接收;

  • 你2591和什么芯片搭配呢

  • 您好,我的代码也是参考basicRf编写的,使用的是cc2530连接2591,但是发现使用2591之后,信号没有明显的放大;

    我只在原先的BascieRf的基础上,在RfInit()中添加了:

    P0SEL&=~BV(7);
    P0DIR|=BV(7);

    AGCCTRL1 = 0x16;
    /* Nothing to be done on radio. */
    /* P1_1 -> PAEN */
    RFC_OBS_CTRL0 = 0x68;
    OBSSEL1 = 0xFB;

    RFC_OBS_CTRL1 = 0x6A;
    OBSSEL4 = 0xFC;

    P0_7=1;

    这一段是我从z-stack中复制出来的,同时按照说明文档写上去的,请问大概的问题在哪里~

    非常感谢!!