This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

关于CC2538 zcl_SendCommand的问题

  我使用的是SampleSwitch和SampleLight范例, Switch是Coordinator,而Light是EndDevice.我的应用是在两者成功进入EZ-MODE之后,Switch会自动连续的发送Toggle command到Light.
  而目前所遭遇的问题是,若连续发送的间隔过短(如100ms), 在发送了几次command之后便会无法再发送该command, 并且Swith会送出Router Request来找寻Light这个装置.但此时Light和Switch之间的Data Request却能正常的feedback.
  在发生上述问题时,只能将Switch或Light断电再开才能恢复.另外若我增加发送command的间隔(如500ms),则能延长问题发生的时间点.故想请问各位,zcl_SendCommand是否有什么限制(例如发送的间隔等等)?