This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
最近在z-stack linux gateway应用上有几个问题,请TI 大神帮忙解答一下:
1.在BeagleBone Black硬件上运行TI提供的网关软件,性能如何衡量?比如说在保证zigbee网络与TCP/IP端服务器正常通信的前提下,一个网关下最多可以部署多少个端点。目前有无其他公司用TI网关方案推出产品。
2.如果做产品将BeagleBone Black和cc2531做到一个PCB上,两者之间还是只能采用USB接口吗?有没有其他选择,对应的软件改动大吗。
3.该方案CC2531的角色应该是协调器吧,但在最新版本z-stack home1.2.2软件包只看到2530和2538文件夹,cc2531模块该下载哪个软件包?
4.要先在硬件平台上搭建linux ubuntu系统,包括USB、网口底层驱动都弄好了,才能安装Z-Stack_Linux_Gateway_1_0_1_installer.run吗?
请帮忙解答一下,谢谢!
1,部署节点的多少,主要跟应用也有关系的。一般作为智能家居的网络,不会超过100个节点的。像Cisco采用这套方案开发的Home Automation Gateway通过ZigBee 认证,并且已经量产了。下面链接是ZigBee官网展示通过认证的产品
http://www.zigbee.org/zigbee-products-2/#zigbeecertifiedproducts/productdetails3/5553fe5ff7f0b6063927b0ef/
2,UART接口就可以。我们演示demo方便就使用的现成的开发板,通过USB来连接,其实这个USB也是虚拟成串口来用的。所以如果直接通过COB的方式做,直接用CC2530,然后串口连接就可以了。
3, 对的,协调器。在ZNP的目录下
4,安装协议栈只要在linux环境下就可以了,一般在PC上进行编译。然后再拿到具体的硬件上运行。如果需要运行的话,驱动肯定是需要的。