This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Zigbee使用的一些问题

Other Parts Discussed in Thread: CC2530

使用产品描述:使用的是CC2530

使用ZHA profile的一些疑问

使用例程:SampleSwitch

函数接口方面疑问:

Q1: EX:通过zclGeneral_SendOnOff_CmdToggle,发送CMD之后。

SampleLight 例程,接受到这个CMD ,会直接调用回调函数(zclSampleLight_OnOffCB)么?

对用户是否是只需要调用zclGeneral_RegisterCmdCallbacks  注册下回调函数即可?

Q2:如何对IP地址的获取,对网点信息的定点发送,有没有profile的的函数可以用。

Q3:profile的attribute是否需要自己改变,还是需要每次手动去修改,比如LED 灯 ON和OFF的状态。

针对Q3:zclSampleLight_OnOffCB    回调函数,只改变了attribute的状态,zclSampleLight_OnOff。是通过改变attribute的状态,然后通过某个函数进行查询,进行LED开关灯操作吗?这个查询函数又在哪调用的。

Q4:现在有一个用了Marvell的zigbee方案的网关,两公司的协议是否可以里连上组网,如果可以需要进行哪些配置,如:是否需要关闭EZ-MODE等

项目较紧,望解答下疑惑谢谢。