各位好
最近试了下加密,但却遇到了一个问题:加密之前设备能正常通信,改成加密之后ED也能入网,但一直不发送任何数据包,加密前后packet sniffer抓取的数据包都在附件里,还请各位帮忙看看是哪里遇到了问题。
加密更改的地方:
-DSECURE=1
-DZG_SECURE_DYNAMIC=0
uint8 zgPreConfigKeys = TRUE
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
各位好
最近试了下加密,但却遇到了一个问题:加密之前设备能正常通信,改成加密之后ED也能入网,但一直不发送任何数据包,加密前后packet sniffer抓取的数据包都在附件里,还请各位帮忙看看是哪里遇到了问题。
加密更改的地方:
-DSECURE=1
-DZG_SECURE_DYNAMIC=0
uint8 zgPreConfigKeys = TRUE
VV 你好
两边的KEY都是默认的,没有作任何修改。
/*********************************************************************
* SECURITY GLOBAL VARIABLES
*/
// This is the default pre-configured key,
// change this to make a unique key
// SEC_KEY_LEN is defined in ssp.h.
CONST uint8 defaultKey[SEC_KEY_LEN] =
{
#if defined ( APP_TP ) || defined ( APP_TP2 )
// Key for ZigBee Conformance Testing
0xbb, 0xbb, 0xbb, 0xbb, 0xbb, 0xbb, 0xbb, 0xbb,
0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa, 0xaa
#else
// Key for In-House Testing
0x00, 0x01, 0x02, 0x03, 0x04, 0x05, 0x06, 0x07,
0x08, 0x09, 0x0A, 0x0B, 0x0C, 0x0D, 0x0E, 0x0F
#endif
};
// This is the default pre-configured Trust Center Link key,
// change this to make a unique key, SEC_KEY_LEN is defined in ssp.h.
CONST uint8 defaultTCLinkKey[SEC_KEY_LEN] =
{
0x56, 0x77, 0x77, 0x77, 0x77, 0x77, 0x77, 0x77,
0x77, 0x77, 0x77, 0x77, 0x77, 0x77, 0x77, 0x77
};
/* Default security key. */
-DDEFAULT_KEY="{0x01, 0x03, 0x05, 0x07, 0x09, 0x0B, 0x0D, 0x0F, 0x00, 0x02, 0x04, 0x06, 0x08, 0x0A, 0x0C, 0x0D}"
我也遇到过同样的问题,现在解决了。因为配置睡眠模式的时候把-DREJOIN_POLL_RATE=440 //default 440改成0了,改回去440后就OK了!