This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

一个CODE 的不理解

void zclLevel_process( uint16 *events )
{
  if ( *events & LEVEL_PROCESS_EVT )
  {
    //update the level
    if(zclLevel_LevelRemainingTime)
    {
      hwLight_ApplyUpdate( &zclLevel_CurrentLevel,
                           &zclLevel_CurrentLevel_256,
                           &zclLevel_StepLevel_256,
                           &zclLevel_LevelRemainingTime,
                           LEVEL_MIN, LEVEL_MAX, FALSE );
。。。。。。。。。

}

进入 hwLight_ApplyUpdate函数

{

。。。。。

 hwLight_Refresh( REFRESH_AUTO );

}

hwLight_Refresh()里有个

#ifdef ZCL_LEVEL_CTRL
  hwLight_UpdateLevel( zclLevel_CurrentLevel );
#endif //ZCL_LEVEL_CTRL

却不能进去。这函数有内有执行呢?(从效果看,应该是执行的,哪里面是什么呢)

  • 已经在另外一个帖子里面回复你了

    1,这个指的是rate,API函数里面是有说明的

    /*********************************************************************
    * @fn zclGeneral_SendLevelControlMoveRequest
    *
    * @brief Call to send out a Level Control Request. You can also use
    * the appropriate macro.
    *
    * @param srcEP - Sending application's endpoint
    * @param dstAddr - where you want the message to go
    * @param cmd - one of the following:
    * COMMAND_LEVEL_MOVE or
    * COMMAND_LEVEL_MOVE_WITH_ON_OFF
    * @param moveMode - LEVEL_MOVE_UP or
    * LEVEL_MOVE_DOWN
    * @param rate - number of steps to take per second
    *
    * @return ZStatus_t
    */
    ZStatus_t zclGeneral_SendLevelControlMoveRequest( uint8 srcEP, afAddrType_t *dstAddr,
    uint8 cmd, uint8 moveMode, uint8 rate,
    uint8 disableDefaultRsp, uint8 seqNum )
    {
    uint8 buf[2];

    buf[0] = moveMode;
    buf[1] = rate;

    return zcl_SendCommand( srcEP, dstAddr, ZCL_CLUSTER_ID_GEN_LEVEL_CONTROL,
    cmd, TRUE, ZCL_FRAME_CLIENT_SERVER_DIR,
    disableDefaultRsp, 0, seqNum, 2, buf );
    }

    2,计算处理PWM的输出,