This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIMAC移植osal_NV遇到问题,需要定义location,求解答

Other Parts Discussed in Thread: TIMAC

环境:IAR版本8303;

开发包:TIMAC;

硬件:CC2530F256

 

将NV操作移植到TIMAC工程中,添加OSAL_Nv.c和.h文件后,编译提示错误:

Fatal Error[e72]: Segment ZIGNV_ADDRESS_SPACE must be defined in a segment definition option (-Z, -b or -P)
 
应该是需要定义location,怎么进行定义?

 

  • 请下载最新的TI MAC协议栈,已经支持NV功能了

    - [6168] Added support for non-volatile (NV) storage. The MAC SampleApp now
    saves network information so it is not lost at device reset. This feature
    can be enabled by the new NV_RESTORE compile flag.