This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

【急】CC2530的P0_7的问题

各位专家,  

我用的协议栈是ZStack-CC2530-2.3.0-1.4.0,请问对于P0_7协议栈里面是否有定义使用?  

我把它设置成输入,用IO中断来检测一个传感器的输入信号,比较奇怪的是如果带着协议栈运行,则输入信号不稳定,会出现周期性的方波;如果去掉协议栈纯粹当单片机使用则正常。

 协议栈代码里的hal_led.h没有include进去,现在还怀疑的一个地方就是mac_radio_defs.h里面的PA/LNA部分,但我在预编译的时候并没有使用。  烦请各位专家帮忙!谢谢!