Other Parts Discussed in Thread: CC2630
由CC2630的数据手册可以看出,在数据发送和接收的时候消耗电流为6mA左右,请问这个器件在维持组网协议中,在不处于数据发送和接收的时候消耗的电流是多少?请问一下表格里面的“Active. Core running CoreMark”代表什么意思啊?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
可以参考CC2630的datasheet
--有源模式 RX:5.9mA
– 有源模式 TX (0dBm):6.1mA
– 有源模式 TX (+5dBm):9.1mA
– 有源模式 MCU:61µA/MHz
– 有源模式 MCU:48.5 CoreMark/mA
– 有源模式传感器控制器:8.2μA/MHz
– 待机电流:1μA(RTC 运行,RAM/CPU 保持)
– 关断电流:100nA(发生外部事件时唤醒)
您好,我想问一下,假如4个CC2630组网,A是主机,BCD是从机,网络组好之后,BCD和A不收发收据的的时候,维持这个网络需要的电流是多大?(3V供电)谢谢!