This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

发送选项的问题.

协议栈版本:2.3.0-1.4.0

协调器打开. 会收到数据.ack正常.

当协调器关闭的时候.

发送选项为

SampleApp_Periodic_DstAddr  = 0x0000;

AF_DataRequest( &SampleApp_Periodic_DstAddr, &SampleApp_epDesc,
SAMPLEAPP_COM_CLUSTERID,
len + 1,
tmp_data,
&SampleApp_TransID,
AF_DISCV_ROUTE | AF_ACK_REQUEST,//需要目的地恢复ACK
AF_DEFAULT_RADIUS ) == afStatus_SUCCESS )

同样会收到ACK.

case AF_DATA_CONFIRM_CMD:
SampleAppAckFailCnt = 0;
if((g_device_info.type == MODEM) || (g_device_info.type == TEST))//只有2种设备
{
HalUARTWrite(0, "Trans", 5);//换行
}
break;

求问这个ACK不是应该由目的地址的 APS发出来的吗?   我希望有一个可靠的 发送-回馈机制. 该怎么做呢?