This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

P_5上电一段时间后自动亮灯不再受控的问题

Other Parts Discussed in Thread: CC2530EM

说明:协议栈是ZStack-CC2530-2.5.1a,

芯片:C2530

现象:1)终端上电大概5分钟,P0_5口自动亮灯,不再受控,其他定义的亮灯IO口都可以控制,在IAR调试模式下,打开寄存器监控,能看到P0_5自动置1,就是不知道是程序在哪里触发的

/* 1 - Green,板载用 */

#define LED1_BV           BV(0) 

 #define LED1_SBIT         P1_0

 #define LED1_DDR          P1DIR

 #define LED1_POLARITY     ACTIVE_HIGH

 /* 2 - Red *板载用*/  

#define LED2_BV           BV(1)

 #define LED2_SBIT         P1_1  

#define LED2_DDR          P1DIR

#define LED2_POLARITY     ACTIVE_HIGH

/* 3 P05,P4蓝灯*/

#define LED3_BV           BV(5)  

#define LED3_SBIT         P0_5     

#define LED3_DDR          P0DIR

#define LED3_POLARITY     ACTIVE_HIGH

  /* 4 P06,P3红灯*/  

#define LED4_BV           BV(6)

#define LED4_SBIT         P0_6     

#define LED4_DDR          P0DIR 

 #define LED4_POLARITY     ACTIVE_HIGH

  /* 5 - P04,P5黄灯*/

  #define LED5_BV           BV(4)  

#define LED5_SBIT         P0_4     

#define LED5_DDR          P0DIR  

#define LED5_POLARITY     ACTIVE_HIGH

问题:1)有没有人知道P0_5是不是协议栈里已经定义他用了,外部不能再使用呀?如何绕开自动触发?

           2)P0_5不受控触发是在ZStack-CC2530-2.5.1a哪里发生的,在IAR上如何操作,很急!断点调试,单步调试都试过,不成功