协议栈是2.5.1-a,想利用热敏电阻接P0_5,以下是我用来读取adc的值
uint16 ReadLightData( void )
{
uint16 reading = 0;
uint16 total = 0;
int i;
P0SEL &= ~0x20;//设置为普通IO
P0DIR &= ~0x20; // 设置P0.5为输入方式
asm("NOP");asm("NOP");
for(i = 0; i < 4; i++)
{
APCFG |= 1 << 5 ; //注意这里是设置ADC输入通道!!
ADCCON3 = 0x80|0x20|0x05; //AVDD5参考电压 10位分辨率 通道5使能
ADCCON1 |= 0x30;//手动模式
ADCCON1 |= 0x40; //开启单通道ADC
while(!(ADCCON1 & 0x80)); //等待AD转换完成
reading = ADCL;
reading |= ((uint16) ADCH) << 8;
reading >>= 6;
total += reading;
}
total >>= 2; //求4次平均值
return total;
}
这样得出来的adc值,在不懂光敏电阻情况下,输出值也是时大时小,有0-1000浮动,本以为adc这东西最简单了,搞了一天都这样,真郁闷!!!