This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2530: ADS1248

Part Number: CC2530
Other Parts Discussed in Thread: ADS1248,

你好!

在使用CC2530加ADS1248测试pt100传感器测温时遇到一个疑问我们所用到的原理与slau520.pdf中比值测试法一致

2.2.1 Ratiometric Measurements 这一章节中的原理 现在没弄明白的是为什么

这个结果里面的2呗关系是怎么得来的 有点没有理解到 能够说明一下吗 非常感谢!

  • 感谢您对TI产品的关注!
    关于你的咨询,我们正在确认你的问题,稍后回复您。

  • 勘误 问题中写了一个错别字2呗 应为2倍

  • 它看起来是因为引用和输入的差异性。 请参阅数据表www.ti.com/.../ads1248.pdf第9.5.2节。
    因为-FS =-Vref / Gain和+FS =+Vref/Gain的代码,所以您可以获得2 * Vref的代码总数。

    t looks like this is because of the differential nature of the reference and input. See section 9.5.2 from the data sheet www.ti.com/.../ads1248.pdf .
    Since you have codes for -FS = -Vref / gain and +FS = +Vref/gain that gives you a total number of codes that are 2 * Vref.

  • 这样解释倒是可以很好的理解,但是实际在应用中我发现我的计算公式中没有体现这个2倍关系也能够将正确的电阻值给计算出来。是因为电阻在采样时得到的值不可能是负值的缘故吗?所以以增益为4倍采样率为20SPS,激励电流为1000微安培时得到电阻值的计算公式为:T_NUM/4/8388607*10000 其中T_NUM为从ADS1248中读取的采样值 10000为参考电阻值为10k欧姆。是我分析的这个原因造成的吗?

    另外我有个疑问就是当激励电流设置成1000微安培,参考电阻值为10k时,产生的参考电压应该是10V还是20V?我实际测量出的电压确是3.6V不知道是什么原因

  • 您是否使用ADS1248电流源(IDAC)生成1mA电流? 如果是,则使用IDAC = 1mA时,REF = 10Kohm是过高的

    此外,您测量的是什么电路? 2线,3线或4线RTD? 如果您正在测量3线RTD,您正在使用多少个IDAC (1x或2x)?

    公式正确。 2的"额外"因子是因为ADC代码范围是双极的,并且从-FS扩展到+FS。 所以满刻度范围(FSR)=+FS --FS = 2*FS

    Are you using the ADS1248 current sources (IDACs) to generate the 1mA current? If so, then RREF = 10kohm is way too high using IDAC = 1mA

    Also, what circuit are you measuring? A 2-, 3-, or 4-wire RTD? If you are measuring a 3-wire RTD, how many IDACs are you using (1x or 2x)?

    The formula is correct. The "extra" factor of 2 comes from the fact that the ADC code range is bipolar and extends from -FS to +FS. So the full-scale range (FSR) = +FS - -FS = 2*FS

  • 上述的问题是针对我们用ads1248采集电阻来转换成温度的项目

    电路是采用的4线制的RTD 只用了一路激励电流源在IEXC1上产生 我们在公式中没有体现这个两倍关系也能得到正确的值 是不是因为我在程序中已经将得到的adc值当成一个有符号的24位数据了 所以公式中就没有体现这个2倍关系。还是说是因为其它原因?

    另外我们还有一种应用场景是用ads1248采集电压来转换压强值的项目

    为了得到的精度我们依然选择使用了和上述一样的设计电路只是我们需要得到电压值但是发现了一些问题就是在计算电压时采取了T_NUM/GAIN*VREF/8388607这样的公式(其中 T_NUM为ADC转换值 GAIN为软件配置的增益VRE计算是通过软件配置的1.5mA电流乘以Rref1.6K 为2.4V 但是实测参考电压为2.056V)就算出来的值与硬件上产生的差分采集电压存在较大的误差即为实际电压的2倍多。出现这个问题是我的计算方式不对吗 还是说原理上理解存在问题?还是说本身这种电路设计就不和理希望得到你的答复 

  • 听起来你并不真正了解RTD的工作原理或ADC的工作原理

    请查看我们的Precision Labs培训材料,了解如何使用精密ADC测量RTD:www.ti.com/.../ti-precision-labs-analogue-to-digital-converters-adcs.html

    此链接指向系列中的第一个视频("RTD简介"),共有11个视频

    他们还可以查看我们的RTD设计指南:www.ti.com/.../sbaa275a.pdf