This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

发包出现漏包的情况

Other Parts Discussed in Thread: CC2530, Z-STACK

环境: Z-stack HA1.2,CC2530

描述:

1. end device 1秒发包一次,coordinator收包,有漏包的情况,10分钟丢失约2-3个包,deivce有编译power saving。

2. 使用sniffer抓包,确认是device端没有发出,但MAC sequence number, 包括APS sequence number都有增加。也就是说数据包“1”发出了之后,下一包变成了“3”,而中间的“2”没有出现,但sequence number有增加表明程序是跑到了发包的地方的。

使用如下命令发包:

AF_DataRequest(&DstAddr, &epDesc, CLUSTERID,10,buffer,TransID,0,AF_DEFAULT_RADIUS);

由于从AF.c往下就是不开放的了,所以请TI的工程师帮忙看一下这是什么情况,谢谢!