Other Parts Discussed in Thread: CC2530
请问下,cc2530的DMA在传输中,如果我要传输一个3成员全是uint32的结构体,那么1个字/字节算一次传输还是传输整个结构体算一次传输?
还有就是,我在配置DMA的时候目的地址的增量如果不是0就不能写入flash,这个怎么搞?
我现在情况是,在写这个结构体的时候flash能被写入但是每个成员都只被写入了第一个字节,搞不懂传输模式跟源/目的地址的增量要怎么配置。
以下是我按ZSTACK配置的代码:
halDMADesc_t *ch = HAL_NV_DMA_GET_DESC(); HAL_DMA_SET_SOURCE(ch, buf); HAL_DMA_SET_DEST(ch, &FWDATA); HAL_DMA_SET_VLEN(ch, HAL_DMA_VLEN_USE_LEN); HAL_DMA_SET_LEN(ch, (cnt * HAL_FLASH_WORD_SIZE)); HAL_DMA_SET_WORD_SIZE(ch, HAL_DMA_WORDSIZE_BYTE); HAL_DMA_SET_TRIG_MODE(ch, HAL_DMA_TMODE_SINGLE); HAL_DMA_SET_TRIG_SRC(ch, HAL_DMA_TRIG_FLASH); HAL_DMA_SET_SRC_INC(ch, HAL_DMA_SRCINC_1); HAL_DMA_SET_DST_INC(ch, HAL_DMA_DSTINC_0); // The DMA is to be polled and shall not issue an IRQ upon completion. HAL_DMA_SET_IRQ(ch, HAL_DMA_IRQMASK_DISABLE); HAL_DMA_SET_M8( ch, HAL_DMA_M8_USE_8_BITS); HAL_DMA_SET_PRIORITY(ch, HAL_DMA_PRI_HIGH); HAL_DMA_CLEAR_IRQ(HAL_NV_DMA_CH); HAL_DMA_ARM_CH(HAL_NV_DMA_CH); FADDRL = (uint8)addr; FADDRH = (uint8)(addr >> 8); // DMA0CFGH =(uint8)(((uint)&dmaCh0) >> 8) & 0x00FF; // DMA0CFGL = (uint8)((uint)&dmaCh0) & 0x00FF; FCTL |= 0x02; // Trigger the DMA writes. while (FCTL & 0x80); // Wait until writing is done.