This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

请问cc2530串口字符串输出大于128字节怎么办?

我用协调器的串口输出字符串,可是字符串太长,大于128了,芯片总是自动重启,请问有什么好办法么?我要发送的字符串是{"method": "response", "result": {"successful": true,"message": "xxxx","data":[{"id":"C1","value":"1"},{"id":"C2","value":"1"}]}}&^!

谢谢

  • 可修改 OnBoard.h内 #define MT_UART_TX_BUFF_MAX 128 #define MT_UART_RX_BUFF_MAX 128 如果想要发送大于128字节的帧而不愿意修改上面的宏,可以在while里面用HalUARTWrite一个字节一个字节的发

  • 可是按照您的修改意见,同时修改 #define MT_UART_TX_BUFF_MAX 128 #define MT_UART_RX_BUFF_MAX 128改为 #define MT_UART_TX_BUFF_MAX 256 #define MT_UART_RX_BUFF_MAX 256会有如下报错,请问这是什么意思?谢谢

    Error[e16]: Segment XDATA_I (size: 0x92 align: 0) is too long for segment definition. At least 0x58 more bytes needed. The problem occurred while processing the  
    segment placement command "-Z(XDATA)XDATA_N,XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available  
    memory ranges were "XDATA:1dc6-1dff"
       Reserved ranges relevant to this placement:
       XDATA:100-3ff        XSTACK
       XDATA:400-1dff       XDATA_Z
       BIT:0-7              BREG
       BIT:80-97            SFR_AN
       BIT:a0-af            SFR_AN
       BIT:b8-c7            SFR_AN
       BIT:d8-df            SFR_AN
       BIT:e8-ef            SFR_AN
    Error while running Linker

  • 可是按照您的修改意见,同时修改 #define MT_UART_TX_BUFF_MAX 128 #define MT_UART_RX_BUFF_MAX 128改为 #define MT_UART_TX_BUFF_MAX 256 #define MT_UART_RX_BUFF_MAX 256会有如下报错,请问这是什么意思?谢谢

    Error[e16]: Segment XDATA_I (size: 0x92 align: 0) is too long for segment definition. At least 0x58 more bytes needed. The problem occurred while processing the  
    segment placement command "-Z(XDATA)XDATA_N,XDATA_Z,XDATA_I=_XDATA_START-_XDATA_END", where at the moment of placement the available  
    memory ranges were "XDATA:1dc6-1dff"
       Reserved ranges relevant to this placement:
       XDATA:100-3ff        XSTACK
       XDATA:400-1dff       XDATA_Z
       BIT:0-7              BREG
       BIT:80-97            SFR_AN
       BIT:a0-af            SFR_AN
       BIT:b8-c7            SFR_AN
       BIT:d8-df            SFR_AN
       BIT:e8-ef            SFR_AN
    Error while running Linker

  • 问题解决没有