This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

cc2530 SPI master + DMA设置的一些问题

在Design Note     DN113的4.1.3 DMA一节的第一段提到:

Even though there is an issue related
to the USARTx TX complete CPU interrupt flag, the only limitation related to using the URX0
and URX1 is that the UxGDR.CPHA bit must be set to zero.

我的问题就是,如果我把2530设置为spi master模式,在发送数据的同时要接收数据。这个时候dma TX req(请求DMA写发送缓冲)没有啥限制,但是如果要

用dma RX req(请求DMA把收到的数据搬走),那么必须把UxGDR.CPHA 设为0???

如果我的外设一定需要CPHA=1才能工作,我又要用DMA来搬收到的数据该怎么办呢??

谢谢!!!