Other Parts Discussed in Thread: CC2530
如题,ZSTACK1.2.0
我在设置32m外部晶振的预定义处改为使用内部16m,发现串口只能发不能收了?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
请问您是如何修改的? CC2530有四个晶振,两个内部(16M RC晶振,32K RC晶振),两个外部(32.768K的石英晶振,32M的石英晶振) 外部的32.768石英晶振也可以不接,但是RF工作时必须选择32MHz crystal oscillator。 建议您最好还是使用32M的晶振
hal_mcu.h文件中
#define CLKCONCMD_32MHZ (CLKSPD(1) | TICKSPD(1) | OSC)
然后hal_board_cfg.h文件中
#define HAL_BOARD_INIT() \
{ \
uint16 i; \ \ SLEEPCMD &= ~OSC_PD; /* turn on 16MHz RC and 32MHz XOSC */ \ while (!(SLEEPSTA & XOSC_STB)); /* wait for 32MHz XOSC stable */ \
asm("NOP"); /* chip bug workaround */ \
for (i=0; i<504; i++) asm("NOP"); /* Require 63us delay for all revs */ \
CLKCONCMD = (CLKCONCMD_32MHZ | OSC_32KHZ); /* Select 32MHz XOSC and the source for 32K clock */ \
while (CLKCONSTA != (CLKCONCMD_32MHZ | OSC_32KHZ)); /* Wait for the change to be effective */ \
/*不关闭内部16M*/ \
/* Turn on cache prefetch mode */ \
PREFETCH_ENABLE(); \
}
急!!!!这是我做的方法,TI方法是???