This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

为什么Ubiqua分别选择16、20和24 channel都能接收到ZLL信号?

敬爱的TI员工,您们好!下面有个问题想请教下您们,希望您们能在百忙之中拨冗指教下,非常感谢!

问题:为什么Ubiqua分别选择11、16、20和24 channel都能接收到ZLL信号??

具体数据见附件,概括描述如下:

1、Ubiqua分别选择11、16、20和24 channel都能接收到ZLL的Touchlink Commissioning Cluster的信号;

2、Ubiqua分别选择16、20和24 channel都能接收到ZLL的on/off Cluster信号。

备注:我只打开一个遥控器和一个ZLight2的灯控模块

multi-channel-received-successfully.zip