This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ADS8332 VA=5V VBD=3.3V时,Vref能不能接2.5V?急!!!

Other Parts Discussed in Thread: ADS8332

ADS8332使用手册中,只看到了VA=2.7 VBD=2.7V  Vreaf=2.5V 或者, VA = 5 V, VBD = 1.65 V to 5 V, VREF = 4.096 V这样的时序图,如我使用VA=5V  VBD=3.3V ,Vref能不能使用2.5V,如果可以那应该是使用哪个时序图?