ADS8332使用手册中,只看到了VA=2.7 VBD=2.7V Vreaf=2.5V 或者, VA = 5 V, VBD = 1.65 V to 5 V, VREF = 4.096 V这样的时序图,如我使用VA=5V VBD=3.3V ,Vref能不能使用2.5V,如果可以那应该是使用哪个时序图?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
谢谢你的建议,我现在遇到一个新问题,ADS8332的SDI脚没办法拉低,只能在1.7V,我在SDI到光耦直接接了一个51欧姆的电阻,测量电阻的另一端也就是光耦脚,电压为0.2V,但是SDI这个脚就是为1.7V,没办法拉低,测量SCLK这个脚就能被拉低,SDI跟SCLK的电路是一样的;
下面是我读取配置信息的代码,但是读出来的都是0xFFFF;