电路如图(参考《基于运算放大器和模拟集成电路的电路设计(第3版)》 384页,峰值检测器一节的做的峰值保持电路),用万用表量第一个运放单元的正端输入3脚和输出1脚,对地都有1伏多的电压,如果把入口处的R92 100k欧的电阻短接到地,1脚输出接近零,但第二个运放单元的输出7脚仍有1伏多电压,怀疑是运放的bias current流经1M欧的大放电电阻所致(手册上该参数只有4.5nA,按说也不应该引起很大的输出误差),把R103换为100k欧,输出电压有所降低,但仍有0.9V左右,(把R99和V27断开,R103短接到地,接接成电压跟随器,7脚输出为零)请问各位专家是什么原因让无输入时,输出不为零,如何消除该直流误差。
![](/resized-image.ashx/__size/550x0/__key/CommunityServer-Discussions-Components-Files/52/0383.1.bmp)