This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
电路如图(参考《基于运算放大器和模拟集成电路的电路设计(第3版)》 384页,峰值检测器一节的做的峰值保持电路),用万用表量第一个运放单元的正端输入3脚和输出1脚,对地都有1伏多的电压,如果把入口处的R92 100k欧的电阻短接到地,1脚输出接近零,但第二个运放单元的输出7脚仍有1伏多电压,怀疑是运放的bias current流经1M欧的大放电电阻所致(手册上该参数只有4.5nA,按说也不应该引起很大的输出误差),把R103换为100k欧,输出电压有所降低,但仍有0.9V左右,(把R99和V27断开,R103短接到地,接接成电压跟随器,7脚输出为零)请问各位专家是什么原因让无输入时,输出不为零,如何消除该直流误差。
你好!
我使用TINA进行了简单的仿真,当我换成+/-15V的时候,输出结果就只有43.47uV,
而使用单电源,则得到741.87mV。
故单双电源对于输入接地测量是有很大影响的,故建议可以试一下采用双电源。而1M的电阻对输出信号有影响,但是影响没那么大,建议可以使用TINA进行简单仿真。
另外,手册上的4.5nA偏置电流是在双电源的条件下测量的。
谢谢!
补充一点,由于datasheet上的测试条件不可能覆盖全部的实际条件,故都可以借助于TINA对应用或者芯片进行仿真,仿真结果一般都跟实际测试结果还是比较接近的。
谢谢!
通过TINA仿真可得到该电路的直流传输特性如下。可以看到该电路只有直流输入电压大于750mV时,输出电压才会比较精确的跟随输入电压。
建议:峰值检测时认为800mV以下的输出皆不是峰值,只检测800mV以上的峰值,则此电路可用。
谢谢大家的指点,之前下载了tina,但一直也没空好好研究如何使用,烦劳各位指条明路,tina如何速成?