This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PGA308: PGA308的输入端过压保护

Part Number: PGA308

请教下,PGA308供电电压为5V,在下图的左端AI_P和AI_N出现30V电压时,PGA308的输入引脚上是否有必要添加钳位二极管,如下图的D12 D13 D14 D15。

我看到数据手册里写了输入引脚上绝对最大电流不超过10mA,绝对最大电压不超过5.3V。如果PGA308内部引脚5和6上没有类似D12 D13 D14 D15这样的钳位二极管(我在手册里没找到类似结构),那30V的高压会直接击穿芯片;