Other Parts Discussed in Thread: LMH6702
6702能否接成差分放大的形式,因为看到6702为电流反馈型
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好!
可以的,datasheet上的电流反馈技术只是反馈的一种拓扑结构,电路是可以完成电压差分放大的。
补充一点,由于你的信号时弱信号,不建议使用LMH6702,因为LMH6702更适合用于驱动,其输出电流范围较大。
能否简述你的应用背景,微弱信号的特点,方便我们推荐更合适的芯片。
谢谢!
请问6702后级是什么?是否用6702做ADC的驱动?如果做ADC的驱动,需要考虑6702的输入offset。由手册第4页可知最大输入offset有6mV,也就是说,接成10倍反向放大组态时,offset会被放大11倍,输出offset会有66mV。如果所处理的信号是一个低通信号,则如此大的offset不可接受;如所处理的信号是一个带通信号,则可以容忍。