Other Parts Discussed in Thread: LM239, LM339, LM2901B, LM339B, LM2901
Dear Madam/Sir,
For LM139AD, there have 3 questions from my side:
- What is the output of LM139AD when input voltage higher than 30V&36V or lower than 2V? If it will lock output of itself.
- What is the output of LM139AD when input voltage in oscillation status? We image worse case, case 1: out of range oscillation, low/high frequency; case 2: within range oscillation, low/high frequency.
- For LM139AD itself failures, can we get the LM139AD failure mode and its impact? For example, failure mode(xxx failure), failure effect(LM139AD output indetermination) this kind of information.
Many thanks for your help.
Sunny Zhao