This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV9151: 数据手册中的电气特性典型值问题

Part Number: TLV9151

你好,

我对数据表中电气特性的“TYP”(典型值)有一些疑问。

首先,在TLV9151的数据表中,第7.3.8节介绍了如何从高斯分布中推导出典型值的方法。像共模抑制比(CMRR)、带宽、噪声等参数,其典型值等于均值(µ);像失调电压(Vos)等参数,其典型值等于均值加上一个标准差(µ + sigma)。我的第一个问题是:这种典型值的方法或标准是否仅适用于此产品(TLV9151),还是可用于TI的所有放大器产品?

其次,如果上述方法能够应用于放大器产品,那么我们就可以将这一结论扩展到数据表中的最小值(MIN)/最大值(MAX)。例如,偏移电压有典型值(TYP)和最大值(MAX),在TLV9151中,典型值为125 µV,最大值为750 µV,分别对应于µ + sigma和µ + 6sigma。我的第二个问题是:如果最大值等于µ + Xsigma,那么如何确定X的值?它是否与生产阶段的过程或筛选测试等条件有关?

第三,在测试阶段,我们需要大量产品来观察偏移电压等指标,然后我们可以将测试结果绘制成如下图所示的分布直方图。在这张图中,我们可以看到它包含了15642个样本,但在其他数据表中,这个数字并不相同。所以我的第三个问题是:在测试阶段,需要多少样本才能充分表征偏移电压等指标的分布?是否有标准规定了测试批量生产的放大器产品的最小采样量?

感谢您的澄清。期待您的回复。

  • 您好

    首先,在TLV9151的数据表中,第7.3.8节介绍了如何从高斯分布中推导出典型值的方法。像共模抑制比(CMRR)、带宽、噪声等参数,其典型值等于均值(µ);像失调电压(Vos)等参数,其典型值等于均值加上一个标准差(µ + sigma)。我的第一个问题是:这种典型值的方法或标准是否仅适用于此产品(TLV9151),还是可用于TI的所有放大器产品?

    不是使用与所有放大器,如原文部分说明,他的举例也仅限于TLV915x,至于其他的放大器没有相关说明。

    其次,如果上述方法能够应用于放大器产品,那么我们就可以将这一结论扩展到数据表中的最小值(MIN)/最大值(MAX)。例如,偏移电压有典型值(TYP)和最大值(MAX),在TLV9151中,典型值为125 µV,最大值为750 µV,分别对应于µ + sigma和µ + 6sigma。我的第二个问题是:如果最大值等于µ + Xsigma,那么如何确定X的值?它是否与生产阶段的过程或筛选测试等条件有关?

    关于这个部分在图Figure 7-9.下面的文字有说明且举了相关例子

    在测试阶段,需要多少样本才能充分表征偏移电压等指标的分布?是否有标准规定了测试批量生产的放大器产品的最小采样量?

    您这个问题当数量增大,在其他条件相同的情况下,只会趋近,无法满足您所说的充分。

    However, process variation and adjustments over time can shift typical means and standard deviations, and
    unless there is a value in the minimum or maximum specification column, TI cannot assure the performance of a
    device. This information should be used only to estimate the performance of a device.