This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV803E: TLV803E在掉电时,为什么会导致输入的VCC更长时间抖动?

Part Number: TLV803E

您好:

     请教个问题,我们使用的完整编码为:TLV803EA43DBZR

我们的应用电路如下:

cid:image002.png@01DC4433.27734980

当没有接监控器件时,P5V_AUX和U145 EN如下波形:(示波器每格400ms)。就是因为P5V_AUX有抖动,导致EN也有抖动,因此,我们才想用监控器件尝试消除EN抖动。

黄色为:P5V_AUX   蓝色为:EN

image.png

 

当接了监控器件后,波形如下:

1.从上电波形来看,是能看到EN延时,说明器件生效了。

2.从掉电波形来看,P5V_AUX抖动时间更长,超出器件延时时间(220ms), 导致EN抖动没有被消除。

 

目前我的疑问:为什么上了监控器件,会导致P5V_AUX抖动时间那么长?这个抖动时间是不是跟延时时间对应,假如我上450ms延时,掉电的抖动时间变成了450ms?如果是这样,我们EN的抖动就没法消除了。

image.png

 

image.png