This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM339電路設計磁帶比較器 問題

Other Parts Discussed in Thread: LM339

請教大家如下問題:

應用:UPS鉛酸電池 過放電保護 (電池規格+12V)

VTH=10.8V

VTL=9.8V

目前設計LM339  OPA 電源VBAT_OP為定電壓+12V電源輸入(電源固定不變),

V_BATTER為電池電壓輸入,測試功能正常。

=========================================================================

問題:若VBAT_OP與V_BATTER都為電池供電,D12設計9V或以下稽納DIODE,

           是否能以下電路或其他設計出VTH=10.8V (高於10.8V輸出HI),VTL=9.8V (低於9.8V輸出LO)?

         實驗測試中,當VBAT_OP電源改為電池,電池降到9.8V,供給OPA電源同時也為9.8V,

         D12稽納DIODE  10V無法穩壓。

  • 当电压VBAT OP低于D12的稳压值时,D12就起不到作用了。如果希望在电池欠压时,还能正常工作,可以采用一个DC-DC将电压升到高于D12的反向电压的水平,并且能保持恒定。电路就会工作了。另一种方案,将电池电压分压后,输入到比较器的正向端。重新设定D12的稳压值,这样就可以在一个低的供电电压下,电路正常工作。