Other Parts Discussed in Thread: TLV1851, TLV7031
我这边为阀片取电设计电路,场景是避雷器氧化锌阀片常态有100uA以上的交流电流经过,使用这个电流为设备功能,实现无内置电池也无外界电源的检测设备。考虑到100uA常态给超级电容充电作为储能,为了防止后端初始化过程中电流高,导致电容电压迅速跌落,低于芯片工作电压,最终初始化反复失败。我准备用TLV3691设计一个滞回电路,靠电容两端电压给滞回电路供电,同时电容电压经过电阻分压后作为比较器输入信号,根据要求我设计了理论上3.6V下门限,4.5V上门限的滞回电路。使用MULTISIM仿真,发现两个问题。首先,当供电的电容电压VCC小于比较器最小工作电压时(0.9V左右),仿真电路的比较器功耗异常高,正常电压下工作电流nA,异常情况有几十到几百uA,且这时候比较器的输出也有异常,正常来说输出应该是接近0V,实际输出接近此时的VCC电压。其次,正常滞回都是当输入信号从0V开始增加,大于上门限时,输出反转,如果接着减少输入信号,当信号小于下门限时,输出才反转。但是仿真情况是当输入信号在上门限和下门限之间时,比较器输出是0V到vcc的振荡,而不是稳定输出。这是怎么回事?是仿真器件模型有问题,还是真实电路也会出现这种情况?