Part Number: XTR305
Other Parts Discussed in Thread: AFE882H1
XTR305没有电流输出,通过下面2方面排查问题如下:
1、不管拆不拆XTR305,AFE882H1输出电压是正常的。
2、把AFE882H1拆掉,用外接电压发生器直接给XTR305电压,7mA以下电流,输出在变化中,不确定。7mA以上是准的。
目前判断是XTR305有些问题,请帮忙看看是不是电路问题?

This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
DAC输出接个缓冲再到XTR305的VIN会更好一些。
对于XTR305输出电流问题,芯片数据手册“Figure 40. Standard Circuit Configuration”是两种模式的电路,“Figure 42”是简单电流输出电路,您再重新确认一下。
您电路中,R44未焊接(即无外接VREF),RSET=1K ,那么Iout=10*VIN mA。负载R28=10欧姆?