This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DRV104能否用于高速开关阀的驱动

Other Parts Discussed in Thread: DRV104

我的高速开关阀需要PWM信号控制其通或断,频率为100HZ左右,24V,1A,DRV104驱动能力达到,但其输出是由PWM转化出的不同电压信号吧?是否能直接输出PWM信号给高速开关阀呢?谢谢。

  • 可以将DRV104输出的PWM信号直接给阀门,考虑到阀门通断频率为100Hz,因而需要根据阀门参数设置合理的延时时间。

  • 我看了关于延时时间的设置说明,谢谢您的答复。我觉得对于100Hz 的高速开关阀,是否应该由单片机输出PWM信号送给不带PWM的普通高边开关来驱动,更适合?您觉得呢?

  • 理论上讲,单片机产生的PWM信号当然可以实现对电磁阀的开关控制,不过需要外扩一个MOSFET实现功率驱动。通常电磁阀的驱动会分为两个过程,快速驱动(高压驱动) 吸合维持(低压保持)。DRV104是专用于此类应用的驱动器件,可以很方便地实现上述过程,单片机只需要输入一个IO电平信号即可。无需关心中间过程以及可能出现的过流、过温等保护。

    我个人感觉DRV104更适合此类应用。