我的高速开关阀需要PWM信号控制其通或断,频率为100HZ左右,24V,1A,DRV104驱动能力达到,但其输出是由PWM转化出的不同电压信号吧?是否能直接输出PWM信号给高速开关阀呢?谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
我的高速开关阀需要PWM信号控制其通或断,频率为100HZ左右,24V,1A,DRV104驱动能力达到,但其输出是由PWM转化出的不同电压信号吧?是否能直接输出PWM信号给高速开关阀呢?谢谢。
理论上讲,单片机产生的PWM信号当然可以实现对电磁阀的开关控制,不过需要外扩一个MOSFET实现功率驱动。通常电磁阀的驱动会分为两个过程,快速驱动(高压驱动) 吸合维持(低压保持)。DRV104是专用于此类应用的驱动器件,可以很方便地实现上述过程,单片机只需要输入一个IO电平信号即可。无需关心中间过程以及可能出现的过流、过温等保护。
我个人感觉DRV104更适合此类应用。