This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

应用于补偿器PID,对于选择运放有什么要求

Other Parts Discussed in Thread: LM6152, LMH6624, OPA4228, INA117, OPA365

应用场合PID补偿器,期望带宽积大于33MHz,失调电压1mV以下,SR在5V/us以上就可以,0.1%的建立时间1us以内,运放输出范围是0~11V,最好是单电源供电。

问题1: 跨导型的运放可以用于PID补偿器吗?

问题2:以高精度运放为例,什么样的运放可以用于PID,应用场合中没有写明用于电源控制,是不是写有应用于滤波器的场合都可以用作补偿器,自己是新手,不太懂,谢谢。

       从高精度运放中选了三个。

  a、LM6152    GBW:75MHz    SR:24V/us   Vos :  2mV    Avo : 94dB

  b、LMH6624   GBW:95MHz    SR:300V/us   Vos :  0.5mV    Avo : 80dB       看到这个运放SR: 300V/us,感觉太高了,这么高的SR对应用于PID有什么负面影响。

 c、OPA221    GBW:45MHz    SR:27V/us   Vos : 0.05mV