This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

vca810放大出现自激

Other Parts Discussed in Thread: VCA810

VCA810电路时按照pdf上的参数手工焊接搭建,输入信号为100mv,放大到8倍以上会出现自己干扰,将原有信号淹没。请问这该怎么办。

  • 你好,能否把你的电路画个图发上来,包括供电和各个电阻电容的值。这样我们才可以分析问题。谢谢。

  • 你好,建议可以先使用TINA对VCA810进行仿真分析,首先要排除电路本身可能造成自激的问题,然后再进一步考虑可能由手工焊接等带来的问题。

    另提供VCA810的参考电路,可供参考和修改,里面有VCA810的模型。

    VCA810.zip
  • 不知你是参考的哪一个电路,自激一般是由输入电容,负载电容和旁路电容引起的。一般会是在信号通路引入了极点。请查找一下,手工焊接过程中的各个连线不要过长。尽量在板上用焊锡连接。尤其注意输入输入端的导线。如果有可能还是做个PCB印制板。

  • 是不是闭环带宽不够了?或者是输出端挂的负载太大了?建议把增益先降下来,或者把输出端负载降低,看看谁否还会有自激出现。

  • 同时注意一下,布局布线,输入在一边,输出在一边。控制信号在侧面。手工焊接搭建电路,引入的问题会比较多。

  • 参照论坛老帖,把VCA810焊接方面注意事项提供给你。

    在指标书的第22页, 有如下说明:

    Socketing a high-speed part like the VCA810 is not

    recommended. The additional lead length and pin-to-pin

    capacitance introduced by the socket can create an

    extremely troublesome parasitic network, which can make

    it almost impossible to achieve a smooth, stable frequency

    response. Best results are obtained by soldering the

    VCA810 onto the board.

    象这样的高速器件,建议你焊接在设计得当的PCB上测试.谢谢!