Other Parts Discussed in Thread: VCA810
VCA810电路时按照pdf上的参数手工焊接搭建,输入信号为100mv,放大到8倍以上会出现自己干扰,将原有信号淹没。请问这该怎么办。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: VCA810
VCA810电路时按照pdf上的参数手工焊接搭建,输入信号为100mv,放大到8倍以上会出现自己干扰,将原有信号淹没。请问这该怎么办。
你好,能否把你的电路画个图发上来,包括供电和各个电阻电容的值。这样我们才可以分析问题。谢谢。
你好,建议可以先使用TINA对VCA810进行仿真分析,首先要排除电路本身可能造成自激的问题,然后再进一步考虑可能由手工焊接等带来的问题。
另提供VCA810的参考电路,可供参考和修改,里面有VCA810的模型。
是不是闭环带宽不够了?或者是输出端挂的负载太大了?建议把增益先降下来,或者把输出端负载降低,看看谁否还会有自激出现。
参照论坛老帖,把VCA810焊接方面注意事项提供给你。
在指标书的第22页, 有如下说明:
Socketing a high-speed part like the VCA810 is not
recommended. The additional lead length and pin-to-pin
capacitance introduced by the socket can create an
extremely troublesome parasitic network, which can make
it almost impossible to achieve a smooth, stable frequency
response. Best results are obtained by soldering the
VCA810 onto the board.
象这样的高速器件,建议你焊接在设计得当的PCB上测试.谢谢!