This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM324正负5V供电,输出电压不对称?

Other Parts Discussed in Thread: LM324

最近用TI的LM324做了一个微分电路,LM324采用正负5V供电,输入信号采用频率400Hz,Vpp=3.3V正弦波。电容利用10nF,可是输出电压居然正负不对称,而且正电压被削平,负电压有振荡。请问这是什么原因?这个电路放大倍数是多少?电路图及仿真波形如下图所示

  • 请问这个电路放大倍数是否可以按如下方法求:

    C6的容抗为Zc=-1/(jwC)=-1/(j*2*pi*f*C)

    输出电压U0=-R5/Zc*Ui=j*2*pi*f*C*R5*Ui;

    带入C=10nF,R5=100KΩ,f=400Hz,得到U0=j*2.512*Ui

    对j*2.512这个数取模得到2.512,即放大倍数为2.512倍,j*2.512还有个幅角影响输出波形相位。

    不知道上述理解正确吗?

    • 在图中所示的位置增加一个电容,输出波形就正常了

  • 能否解释一下在不加电容C2 10n输出电压为什么不对称?而且输出还有正弦波掺杂在里边。

    加上电容C2原因?

    对于这个电路放大倍数是否可以按如下方法求:

    C6的容抗为Zc=-1/(jwC)=-1/(j*2*pi*f*C)

    输出电压U0=-R5/Zc*Ui=j*2*pi*f*C*R5*Ui;

    带入C=10nF,R5=100KΩ,f=400Hz,得到U0=j*2.512*Ui

    对j*2.512这个数取模得到2.512,即放大倍数为2.512倍,j*2.512还有个幅角影响输出波形相位。

    不知道上述理解正确吗?